Beli raspberry pi di monotaro.id
Kami Menampilkan Rekomendasi Kami Untuk Anda! Anda Bisa Membelinya Kapan Saja di monotaro.id
- Phoenix Contact Power Supply UnitDeskripsi:Four-channel, redundant fieldbus power supply base. Host connection is a D-SUB 25 socket connector.
- Raspberry Pi FPC Display Cable (200mm) for Raspberry Pi 5Deskripsi:This cable is for connecting a DSI display to a Raspberry Pi 5. The cable must be connected to one of the two 4-lane MIPI connectors on the Raspberry Pi 5.atribut:
- Length (mm): 200
- Kyohritsu Electronic Industry Raspberry Pi 4 Model B Single Board Computer with 8GB SD Card and Raspberry Pi OS Pre-Installed (Modul Komputer)Deskripsi:This set includes the Raspberry Pi 4 and an SD card with the latest OS written to it. The latest generation of the single-board computer Raspberry Pi, the Raspberry Pi 4 Model B, is here! While maintaining the same board size as previous models in the series, the new model boasts major performance improvements, including an ARM Cortex-A72 quad-core CPU and 4K display output, making learning programming and building embedded systems more convenient and flexible. Wi-Fi and Bluetooth have obtained the necessary technical approval for use in Japan. The latest OS, "Raspberry Pi OS (32-bit) with Desktop and Recommended Software," is already installed on the SD card (microSD), so simply inserting this product into your Raspberry Pi will immediately start up the OS. [SD card product overview] This is an SD card with the latest OS for Raspberry Pi written on it. Installing an OS on a Raspberry Pi requires a separate PC and software, The process of getting the Raspberry Pi up and running takes some time, including installation. If you're not used to it, it can be a surprisingly difficult task. This product comes with the latest OS, "Raspberry Pi OS (32-bit) with Desktop and Recommended Software," pre-installed on the SD card (microSD), so simply inserting the product into your Raspberry Pi will immediately start up the OS. This will free you from the hassle of startup work. [Set contents]・Single board computer Raspberry Pi 4 Model B・32GB microSDHC card (with SD adapter/Raspberry Pi OS installed) [Features] CPU The CPU core of the Raspberry Pi 4 Model B has been upgraded from the ARM Cortex-A53 to the Cortex-A72, improving processing performance per clock. The operating clock speed has also been increased from 1.4GHz to 1.5GHz. Most programs will run as is. memory The Raspberry Pi 4 Model B comes with 1GB of main memory, the same as the previous Raspberry Pi 3 Model B+/B, as well as versions with expanded memory of 2GB, 4GB, and 8GB. Ethernet (wired LAN) The previous Raspberry Pi 3 Model B+ had a Gigabit Ethernet-compatible LAN controller connected via USB 2.0, which limited the theoretical maximum transfer speed to 300 Mbps. However, the Raspberry Pi 4 Model B has a changed controller and connection interface, which enables even faster transfer speeds. Bluetooth (near field communication) The Raspberry Pi 4 Model B now supports the Bluetooth version 5.0 standard, improving communication speed and distance. HDMI video output The Raspberry Pi 4 Model B now supports HDMI video output at 4K (3,840 x 2,160) resolution at 60 frames per second thanks to the enhanced graphics performance of the SoC. It also comes equipped with two HDMI connectors, allowing dual-screen output. The connector shape has been changed from full-size HDMI (Type A) to Micro HDMI (Type D). case The Raspberry Pi 4 Model B has the same board size as the previous Model B series, but there are changes to the connector types and layout, so depending on the case structure, products for the previous model may not be compatible. Internal Interface The internal interfaces of the Raspberry Pi 4 Model B, such as the GPIO pin header, CSI camera port, and DSI video port, remain unchanged from the Pi 3/2/B+. power supply The power input connector for the Raspberry Pi 4 Model B has been changed from USB Type B Micro (micro USB) to Type C. Also, because power consumption has increased with the improved performance, it is recommended to use a power supply capable of outputting 3A.*Please note that the SD card (microSD) may differ in manufacturer name and whether it comes with or without an SD card conversion adapter depending on when it was installed. ※Please note: *Please note that the OS version may change over time. *Please note that users are free to upgrade their OS if necessary. *Some product contents may change depending on the arrival date. *Set contents may change without notice. *Wi-Fi and Bluetooth have obtained the technical standards required for use in Japan. *[Points to note when purchasing Raspberry Pi 4] *Please prepare a new power cable for the Raspberry Pi 4* Starting with the Raspberry Pi 4, power is provided via a USB C connector. * Conventional AC adapters cannot be used. Please use the "AC adapter DC5V 3A (USB-C) / UU318-0530." *Please prepare a new HDMI cable for the Raspberry Pi 4* With the Raspberry Pi 4, the video output has changed from HDMI to micro HDMI. * Conventional HDMI cables cannot be used. Please use the "HDMI Cable AD (micro) 1m [RoHS] / 2HDMI-10M." *Please prepare a case for the Raspberry Pi 4. *The power and HDMI connectors have changed since the Raspberry Pi 4. * Conventional cases cannot be used, so please use the "Raspberry Pi 4 case." *A fan is essential for high-load processing, so please prepare a new one* The Raspberry Pi 4 has significantly improved performance, but in exchange, it generates very high temperatures. *When high CPU power processing is required, such as deep learning or video processing, be sure to take heat countermeasures such as using a fan and heat sink to ensure the device performs at its best.atribut:
- Audio Output: Stereo: DIA3.5mm 4-pole jack HDMI: Shared with video output I2S pin header
- Bluetooth: 5.0/BLE
- Main Unit: 8GB version
- Maximum Power Consumption (W): About 15
- Memory: (LPDDR4)8GB
-
Output:
Video: 2 x HDMI 2.0 Type D (Micro HDMI) video/audio sockets
Composite video (PAL/NTSC) output: DIA3.5mm 4-pole jack Display interface: DSI - Power Supply: 5V 3A (USB Type C)
- ROHS Directive (Corresponding to 10 Substances): Correspondence
- Size: 56(W)x85(D)x17(H)mm
- Storage: microSD memory card (SDIO)
- Suitable CPU: 64bit 1.5GHz quad core ARM Cortex-A72
- USB Port: 2(USB3.0)+2(USB2.0)
- Wi-Fi: IEEE 802.11 b / g / n / ac 2.4 / 5GHz dual band
- Raspberry Pi Raspberry Pi 5 FPC Camera CableDeskripsi:This is the official Camera Interface (CSI) cable for models with a 22-pin CSI connector, such as the Raspberry Pi 5. In the case of conventional models, the standard on the main body is 15 pins, so the cables that came with previous camera products may not be compatible. In that case, please use this cable.*This product cannot be used to connect to a display because the wiring is different from that of a display cable (DSI interface).atribut:
- Suitable Model: Raspberry Pi 5,Zero 2 W,Zero(W),Compute Module 4 I/O Board
- Terminal Shape: [Camera side] 15P 1.0mm pitch
- Raspberry Pi Raspberry Pi 4 Model B/8GBDeskripsi:The Raspberry Pi 4 Model B offers significant upgrades over its predecessor, the Raspberry Pi 3 Model B+, including CPU, RAM, USB, and networking. This product is an 8GB model that complies with the Technical Standards Certification (GITE). CPU: The Raspberry Pi 4 Model B's CPU uses the ARM Cortex-A72 architecture and operates at 1.5GHz. RAM: While the Raspberry Pi 3 Model B+ only had a 1GB model, an 8GB model has been added to the lineup. The RAM standard has also been upgraded from DDR2 to DDR4. Video Output/GPU: The video output connector has been upgraded from one full-size HDMI (Type A) port to two micro HDMI (Type D) ports, allowing for dual-screen output. The GPU has been upgraded from VideoCore IV to VI, adding support for 4K60p, H.265 decoding, OpenGL ES 3.0, and more. Ethernet (Wired LAN) Gigabit Ethernet (wired LAN) speeds have also been significantly increased from 300Mbps via USB 2.0 on the Raspberry Pi 3 Model B+ to 1000Mbps (logical). Bluetooth: Bluetooth 5.0 has been upgraded from Bluetooth 4.2. USB Interface: The Raspberry Pi 3 Model B+'s four USB 2.0 ports have been upgraded to two USB 3.0 ports and two USB 2.0 ports. Power: The power input connector has been upgraded to USB Type-C, allowing for higher current. Power requirements have also been increased to 5V/3A. Compatibility: The Raspberry Pi 4 Model B has changed its video output and power connector, resulting in some incompatibility with some options, such as cases and AC adapters. The size, shape, and GPIO pin specifications have not changed, so most HATs and modules can be used with the previous model.Specifications may differ from the actual product depending on the manufacturing date and lot. Please use Raspbian 2019-06-20 and NOOBS 3.1.1 (2019-06-24) or later. The wireless LAN function is disabled by default. It can be enabled by setting the country of use.atribut:
- Audio Output: 3.5mm 4-pole jack, HDMI (shared with video output), I2S pin header
- Bluetooth: Bluetooth 5.0, Bluetooth Low Energy
- Correspondence to Ethernet: 10/100/1000 Base-T RJ45 Socket (BCM54213PE)
- Country of Origin: United Kingdom
- Dimensions (mm): 85x56x17
- Maximum Power Consumption (W): About 15
- Memory: 8GB DDR4-2400 low-voltage SDRAM
- Output: [Video] Two micro HDMI (Type D) ports, composite 3.5mm 4-pole jack (PAL, NTSC), DSI
- Power Supply: USB Type C Socket 5V 3.0A / 2.54mm Pin Header / PoE (Requires optional PoE HAT)
- Suitable CPU: 1.5GHz quad-core Cortex-A72 (ARMv8, 64bit L1=32KB, L2=1M)
- Wi-Fi: IEEE 802.11 b/g/n/ac 2.4/5GHz
- RS PRO Raspberry Pi Aluminum Case for Raspberry Pi (Casing Modul Komputer)atribut:
- ROHS Directive (Corresponding to 10 Substances): Correspondence
- SUNHAYATO SOP IC conversion board (1.27mm pitch/max. 28 pins)Deskripsi:This board can convert SOP ICs up to 28 pins into 2.54mm pitch. It is a universal board for converting SOP (Small Outline Package) ICs up to 28 pins from 1.27mm pitch to 2.54mm pitch. It is very useful for prototyping and evaluation when you want to mount SOP package ICs on a universal board. It supports up to 28 pins. There are three identical patterns on one board, and the V-cut processing makes it easy to separate. SOP ICs can be mounted on standard 2.54mm pitch universal boards. Gold flash plating and double-sided resist make it highly reliable and RoHS compliant.atribut:
- ROHS Directive (Corresponding to 10 Substances): Correspondence
- Raspberry Pi Raspberry Pi Touch Display 2Deskripsi:This is the official Raspberry Pi 7-inch touch panel display. The screen resolution has been increased from the previous model to 1280 x 720 dots (800 x 480 on the previous model), and it has multi-touch functionality with up to 5 points. It is used by connecting to the DSI interface on the Raspberry Pi board. The Raspberry Pi itself can be fixed to the back of the display to form an integrated structure. The screen can be rotated using software, allowing it to be used in either landscape or portrait orientation. Power can be supplied from the Raspberry Pi's GPIO connector, so no additional power supply is required. Compatible with most Raspberry Pi models except for the earliest models and the Zero series. [Set contents] Touch Display 2 body fixing screws (8 pieces) FFC cable: 15P-15P *For Raspberry Pi 4 and earlier FFC cable: 15P-22P *Power supply cable for Raspberry Pi 5atribut:
- Color: 24-bit RGB
- Conform to: Touch: Up to 5-point multi-touch
- Dimensions (mm): 7 type (display area: 155 x 88)
- Interface: DSI
- Resolution: 1280 x 720 dots
- Suitable Model: Raspberry Pi (1 A+/B+ or later) *Excluding the Zero series (without expansion connectors)
- GOSAVE Road Barrier (Barikade Jalan)atribut:
- Color: Orange
- Material: HDPE
- Origin: China
- Size (cm): 115x26x67
- Autonics Slim Remote I/O ARIO SeriesDeskripsi:The ARIO series slim remote I/O offers Ethernet/Fieldbus communication I/O with modular expansion up to 64 units in various I/O types. The coupler modules are available in various communication protocols. The push-in connection method offers simple and easy wiring for improved user convenience. The hot-swap feature allows the terminal unit and body (control) unit of the module to be disconnected from the base (communication) unit without stopping power or communication for easy maintenance.atribut:
- Humidity Level: 35-85%RH, enclosed space: 35-85%RH
- Material: Terminal: polyamide6, Body: modified polyphenylene oxide, Base: polyamide6, poly oxy methylene
- Mounting Type: DIN rail mounting
- Certification: CE
- Environment Temperature Level (°C): -10 to 55, enclosed space: -25 to 70
- Chitose Meeting Chair Daishogun Bold (Kursi Kantor / Rapat)atribut:
- Dimensions (WxDxH) (mm): 449x493x807
- Seat Height (mm): 455
- Upholstery Materials: Fabric
- Frame Finishing: Powder Coating
- TEKIRO Combination Wrench Metric (Kunci Ring Pas)Deskripsi:TEKIRO KUNCI RING PASKegunaan dari kunci Kombinasi ini adalah saling mengisi kekurangan yang ada pada masing masing kunci pas dan ring. Kunci ini sangat berguna saat menyetel pengikat (fastener) dengan ukuran yang sama pada posisi yang berbeda.Kunci Kombinasi merupakan gabungan dari kunci pas dengan kunci ring pada masing masing ujung dengan ukuran yang sama. Kunci pas ujung terbuka hanya dapat digunakan bila kunci pas berbentuk cincin atau soket tidak cocok dengan kepala baut atau mur.Fungsi : Kegunaan dari kunci Kombinasi ini adalah saling mengisi kekurangan yang ada pada masing masing kunci pas dan ring. Kunci ini sangat berguna saat menyetel pengikat (fastener) dengan ukuran yang sama pada posisi yang berbeda.
- SAFETY JOGGER Sepatu Safety Sneakers High Cut Desert S1P (Sepatu Proyek)Deskripsi:Sepatu pengaman bergaya dengan bagian atas kanvas. Perkenalkan sepatu pengaman DESERT yang serbaguna, yang dirancang untuk para pekerja keras. Sepatu pengaman dengan harga menengah ini bukan sekadar alas kaki, tetapi menjanjikan keamanan dan kenyamanan yang tak tertandingi. Anti selip menawarkan cengkeraman yang kuat di berbagai permukaan, cocok untuk aplikasi otomotif, logistik, industri, dan konstruksi. Bagian ujung sepatu dan midsole yang terbuat dari baja yang kokoh melindungi kaki Anda dari benda-benda yang jatuh dan penetrasi yang tajam, sementara fitur anti-statis melindungi dari penumpukan elektrostatis. Sepatu DESERT juga menawarkan pereda nyeri dari postur tubuh dan menjaga kaki Anda tetap sejuk dan segar sepanjang hari. Dengan bagian atas kanvas yang bergaya yang tersedia dalam warna hitam, biru atau pasir, sepatu ini lebih dari sekadar sepatu pengaman - sepatu ini adalah pernyataan gaya.- Pelindung jari kaki- Alas kaki yang dapat dilepas- Pemasangan ortopedi (Neskrid)- Midsole anti-lubang- Bernapas- Anti selip- Mencegah percikan api atau muatan statis- Overnoseatribut:
- Series: Desert-011 S1P
- Approval: ASTM F2413:2024, EN ISO 20345:2011
- Category: S1 P / SRC
- Footbed: SJ foam footbed
- Lining: Cotton
- Midsole: Steel
- Outsole: PU/PU
- Toecap: Steel
- Upper: Cotton
- Raspberry Pi Raspberry Pi Zero 2 WHDeskripsi:This is the latest addition to the Raspberry Pi Zero family, featuring the Raspberry Pi RP3A0 SiP, centered around a 1 GHz 64-bit Arm Cortex-A53 quad-core BCM2710A1 die with 512MB of RAM. Compared to the previous Raspberry Pi Zero, single-threaded performance is 40% better and multi-threaded performance is 5x better. 2.4 GHz 802.11 b/g /n wireless LAN and Bluetooth 4.2 / Bluetooth Low Energy (BLE) are available.*Construction design certification (technical conformity certification) has been completed. The certification is printed on the package, so please do not throw away the package and keep it.atribut:
- Bluetooth: 4.2
- Board Dimensions (mm): 65 x 30 (height max 5.2
- Mass (g): About 10
- Operating Temperature (°C): -20~+70
- Suitable CPU: Broadcom BCM2710A1, quad-core 64-bit SoC (Arm Cortex-A53@1 GHz)
- Video Output: Mini HDMI
- Wi-Fi: 802.11b/g/n
- Snap-on Combination Wrench Flank Drive Plus Metric (Kunci Ring Pas)atribut:
- Style: 12-point
- ASME: B107.100
- Country of Origin: USA
- Finish: Chrome
Daftar Harga raspberry pi Terbaru October 2026
| Phoenix Contact Power Supply Unit | Rp819.900 |
| Raspberry Pi FPC Display Cable (200mm) for Raspberry Pi 5 | Rp61.900 |
| Kyohritsu Electronic Industry Raspberry Pi 4 Model B Single Board Computer with 8GB SD Card and Raspberry Pi OS Pre-Installed (Modul Komputer) | Rp9.999.900 |
| Raspberry Pi Raspberry Pi 5 FPC Camera Cable | Rp84.900 |
| Raspberry Pi Raspberry Pi 4 Model B/8GB | Rp9.499.900 |
| AS ONE Case Optional Parts For Raspberry Pi | Rp209.900 |
| RS PRO Raspberry Pi Aluminum Case for Raspberry Pi (Casing Modul Komputer) | Rp1.899.900 |
| SUNHAYATO SOP IC conversion board (1.27mm pitch/max. 28 pins) | Rp269.900 |
| Raspberry Pi Raspberry Pi Touch Display 2 | Rp3.699.900 |
| GOSAVE Road Barrier (Barikade Jalan) | Rp599.900 |
Data diperbarui pada 10/10/2026 (Harga belum termasuk PPN)




















































































































































%20for%20Raspberry%20Pi%205/nsP116522856-1.jpg)
/35P115165113-1.jpg)



/naP115402838-1.jpg)
/eeP115175518-1.jpg)

%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Alat%20Keselamatan%20Kerja/Kerucut%20Jalan/Barikade/GOSAVE%20Road%20Barrier%20(Barikade%20Jalan)/3kP112397128-1.jpg)

/bdP107418409-1.jpg)
/60P101000216-6.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sepatu%20Safety/Sepatu%20Safety%20Sneaker/Sneaker%20Safety%20High%20Cut/SAFETY%20JOGGER%20Sepatu%20Safety%20Sneakers%20High%20Cut%20Desert%20S1P%20(Sepatu%20Proyek)/1jP102038055-3.jpg)
/2wP101519104-149.jpg)

/rlP103252993-1.jpg)
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
/WD-40%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20333ml%201pc/60S000055216-2.jpg)
/OLFA%20Cutter%20Knife%20Safety%20(Pisau%20Cutter)%20149B%201pc/S009054721-2.jpg)
/Joyko%20Gel%20Ink%20Pen%20Q%20(Pulpen%20G2%20%2F%20Pulpen%20Gel)%20GP-265%20Black%200_5mm%201box(12pcs)/qmS009904958-2.jpg)
/REXCO%20Multi-Purpose%20Lubricant%20(Pelumas%20Serbaguna)%20RX-SP0009%20500ml%2F415g%201pc/2bS000076083-4.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Sarung%20Tangan/Sarung%20Tangan%20Tahan%20Minyak/Sarung%20Tangan%20Tahan%20Minyak%20Karet%20Nitril/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)/ANSELL%20Gloves%20Solvex%20Nitrile%20(37-176)%20(Sarung%20Tangan%20Nitrile%20Anti%20Kimia)%2037-176%20Size%209%201pair/S000074366-1.jpg)

%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)/IKA%20(Copy%20Paper)%20Copy%20Paper%20A4%2070gsm%20(Kertas%20HVS%20%2F%20Fotocopy)%20IKF%20PC%2070%20A4G%201ream/8pS035166313-2.jpg)
%2C%20Perlindungan%20Diri%20%26%20Kesehatan/Kesehatan/Pertolongan%20Pertama%2C%20Kebutuhan%20Higienis/Perban%2C%20Kain%20Kasa/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)/OneMed%20Alkohol%20Swab%20(Tisu%20Alkohol)%201box(100pcs)/h6S039287618-2.jpg)
/3M%20Post-it%20654%20Sticky%20Notes%20(Kertas%20Memo)%20654-5CY%201pack(5pads)/5iS030245198-4.jpg)
/monotaro_id%20Lakban%20OPP%202inch%20(Solasi%20%2F%20Selotip)%20Transparent%2048mmx64m%201roll/h7S036166619-4.jpg)

/monotaro_id%20Cable%20Ties%204_8x250mm%20(Pengikat%20%2F%20Kabel%20Tis)%20White%201pack(100pcs)/2xS039549105-2.jpg)
/Max%20Stapler%20Needle%20(Isi%20Staples)%20No_10-1M%205%2F16x3%2F16Inch%201pack(20pcs)/S000005230-4.jpg)
/monotaro_id%20Plas%20Chamois%20(Lap%20Kanebo)%20with%20tube%20Yellow%2032x21cm%201pc/4uS037754174-2.jpg)